4.36 Ifndef Directive
The MPASM IFNDEF directive begins a conditional block of
assembly code.
Suggested Replacement
#ifndef preprocessor directive can be used as a replacement for
this directive, as shown in the example below. Ensure the assembly source file uses
a .S extension so that it will be preprocessed by the assembler.
For
example:#ifndef RUNMODE
movf state,w
call diag
#endifAlthough the MPASM assembler allows you to use a
#IFNDEF form of this directive, note that it is still an
assembler directive. The PIC Assembler's #ifndef directive is a
preprocessor directive, hence will be looking for the definition of a
preprocessor symbol, not an assembler symbol. If you migrate your
code to use the preprocessor directive, ensure that you also define as required the
equivalent preprocessor macros using either the#define directive or
-D option.