4.18 Dw Directive
The MPASM DW directive places words into program memory.
Suggested Replacement
The PIC Assembler's DW directive inside a suitable
psect performs a similar function, but there are some differences in its
operation.
This directive places the value of its comma-separated operands as 16-bit words into
the current psect. For PIC18 devices, each operand will consume two addresses
(bytes). For other devices, the assembler will attempt to place the entire operand
value into one program memory word, but since program memory locations of these
devices are less than 2 bytes wide, the value may be truncated. Typically, data is
stored in the program memory of these devices using retlw
instructions that store each byte in separate memory locations.
If the operand is a string literal, each character of the string is stored sequentially as a 16-bit word, with no terminating nul character.
You can use the data psect to hold the values defined.
This psect is predefined once you include <xc.inc>. For
example:
PSECT data
modifiers:
DW 1354h
DW 's', -23
DW 'Mode'
space flag is set to 0 (the default value).
It can be assigned an address by associating it with a suitable linker class (e.g.
CONST for PIC18 devices, or STRCODE for other
devices), or by explicitly positioning the psect using the linker's
-P option (accessible from the driver using the
-Wl option), as in the following PIC18
example.PSECT myData,space=0,class=CONST
modifiers:
DW 1354h
DW 's', -23
DW 'Mode'