4.35 Ifdef Directive
The MPASM IFDEF directive begins a conditional block of
assembly code.
Suggested Replacement
#ifdef preprocessor directive can be used as a replacement for
this directive. Ensure the assembly source file uses a .S extension
so that it will be preprocessed by the assembler. For
example:#ifdef DBG
movf state,w
call diag
#endifAlthough the MPASM assembler allows you to use a #IFDEF
form of this directive, note that it is still an assembler directive. The PIC
Assembler's #ifdef directive is a preprocessor directive,
hence will be looking for the definition of a preprocessor symbol, not an
assembler symbol. If you migrate your code to use the preprocessor
directive, ensure that you also define as required the equivalent preprocessor
macros using either the#define directive or -D
option.