4.15 #define Directive
The MPASM #DEFINE directive defines textual replacement for
a macro.
Suggested Replacement
As assembly source files can be preprocessed, the
#define preprocessor directive (case sensitive) can be used as
a direct replacement for this assembler directive, as shown in the example
below.
All the usual preprocessor features associated with macro replacement are available.
Ensure the assembly source file uses a .S extension so that it will
be preprocessed by the assembler, or alternatively, use the
-xassembler-with-cpp option to request that source files be
preprocessed regardless of their extension.
#define SUMSP(a, b) (a+2*b)
PSECT code
process:
movlw SUMSP(5, 3)
movwf volume
...