4.13 Db Directive
The MPASM DB directive places bytes into program memory.
Suggested Replacement
The PIC Assembler's DB directive inside a suitable
psect performs a similar function, but there are some differences in its
operation.
This directive places the value of its comma-separated operands as bytes into the current psect. If the operand is a string literal, each character of the string is stored sequentially, with no terminating nul character.
With PIC18 devices, each byte specified will consume one byte of program memory. With
Mid-range devices, there will be one byte stored in each program word, with the
upper bits of that word left as zeros. To have data encapsulated into
retlw instructions, use retlw instructions
instead of this directive (see the example in the Dt Directive).
data psect to hold the values defined. This psect is
predefined once you include <xc.inc>. For
example:PSECT data
symbols:
DB 76h
DB 'A', -23
DB "Message",0Alternatively, you can define your own psect and allocate it to program
memory. Ensure that the psect's space flag is set to 0 (the default
value). It can be assigned an address by associating it with a suitable linker class
(e.g. CONST for PIC18 devices, or STRCODE for
other devices), or by explicitly positioning the psect using the linker's
-P option (accessible from the driver using the
-Wl option), as in the following PIC18 example.
PSECT romData,space=0,class=CONST
symbols:
DB 76h
DB 'A', -23
DB 'Message",0