4.3 Bankisel Directive
On Mid-range devices only, the MPASM BANKISEL directive generates
bank selection code appropriate for indirect access of the register address specified by
its argument.
Suggested Replacement
No change is necessary; continue to use the BANKISEL assembler
directive.
This directive is case-insensitive, can be used with any device, and works with
numeric or symbolic operands. Note that it may generate more than one instruction,
so it should not be used immediately following any test-and-skip instruction. If the
directive is used with a device that does not require bank selection code for
indirect access (for example, a PIC18 device) a warning is issued and the directive
is ignore.
movlw myVar
movwf FSR ;load the address of myVar info FSR
BANKISEL myVar ;select the correct bank for myVar
movlw 055h
movwf INDF ;indirectly write to myVar