3.9.3 PLL Enable State Machine
The PLL enable state machine starts the PLL for RX, TX or temperature measurement. Depending on the configuration of SSMTX and SSMTM in the SSMCR register, the LNA is additionally enabled (see the following table).
If SSMTM is set, this state machine enables the temperature mode in the RF front end.
As a plausibility check, the XRDY flag in the FESR is expected to be set to
‘1’ to ensure that the XTO is up and running. If this check is not
successful, the sequencer state machine ends with the error flag set.
Usually, the PLL enable state machine is the first entry in a setup sequence to start RX or TX. It can be followed by the VCO tuning or immediately followed by the PLL lock state machine if no tuning is required.
|
Setting |
Description |
|---|---|
|
SSMCR.SSMTX |
Depending on these settings, the state machine decides whether to enable the LNA or not. |
|
SSMCR.SSMTM |