32 Instruction Set Summary
The dsPIC33C instruction set is almost identical to that of the dsPIC30F and dsPIC33F.
Most instructions are a single program memory word (24 bits). Only three instructions require two program memory locations.
Each single-word instruction is a 24-bit word, divided into an 8-bit opcode, which specifies the instruction type and one or more operands, which further specify the operation of the instruction.
The instruction set is highly orthogonal and is grouped into five basic categories:
- Word or byte-oriented operations
- Bit-oriented operations
- Literal operations
- DSP operations
- Control operations
Table 1 lists the general symbols used in describing the instructions.
The dsPIC33 instruction set summary in Table 32-2 lists all the instructions, along with the status flags affected by each instruction.
Most word or byte-oriented W register instructions (including barrel shift instructions) have three operands:
- The first source operand, which is typically a register ‘Wb’ without any address modifier
- The second source operand, which is typically a register ‘Ws’ with or without an address modifier
- The destination of the result, which is typically a register ‘Wd’ with or without an address modifier
However, word or byte-oriented file register instructions have two operands:
- The file register specified by the value ‘f’
- The destination, which could be either the file register ‘f’ or the W0 register, which is denoted as ‘WREG’
Most bit-oriented instructions (including simple rotate/shift instructions) have two operands:
- The W register (with or without an address modifier) or file register (specified by the value of ‘Ws’ or ‘f’)
- The bit in the W register or file register (specified by a literal value or indirectly by the contents of register ‘Wb’)
The literal instructions that involve data movement can use some of the following operands:
- A literal value to be loaded into a W register or file register (specified by ‘k’)
- The W register or file register where the literal value is to be loaded (specified by ‘Wb’ or ‘f’)
However, literal instructions that involve arithmetic or logical operations use some of the following operands:
- The first source operand, which is a register ‘Wb’ without any address modifier
- The second source operand, which is a literal value
- The destination of the result (only if not the same as the first source operand), which is typically a register ‘Wd’ with or without an address modifier
The MAC class of DSP instructions can use some of the
following operands:
- The accumulator (A or B) to be used (required operand)
- The W registers to be used as the two operands
- The X and Y address space prefetch operations
- The X and Y address space prefetch destinations
- The accumulator write-back destination
The other DSP instructions do not involve any multiplication and can include:
- The accumulator to be used (required)
- The source or destination operand (designated as Wso or Wdo, respectively) with or without an address modifier
- The amount of shift specified by a W register ‘Wn’ or a literal value
The control instructions can use some of the following operands:
- A program memory address
- The mode of the Table Read and Table Write instructions
Most instructions are a single word. Certain double-word instructions are
designed to provide all the required information in these 48 bits. In the second word, the
eight MSbs are ‘0’s. If this second word is executed as an instruction (by
itself), it executes as a NOP.
The double-word instructions execute in two instruction cycles.
Most single-word instructions are executed in a single instruction cycle,
unless a conditional test is true or the Program Counter is changed as a result of the
instruction, or a PSV or Table Read is performed. In these cases, the execution takes
multiple instruction cycles, with the additional instruction cycle(s) executed as a
NOP. Certain instructions that involve skipping over the subsequent
instruction require either two or three cycles if the skip is performed, depending on
whether the instruction being skipped is a single-word or two-word instruction. Moreover,
double-word moves require two cycles.
| Field | Description |
|---|---|
| #text | Means literal defined by
“text” |
| (text) | Means “content of
text” |
| [text] | Means “the location addressed by
text” |
| { } | Optional field or operation |
| a ∈ {b, c, d} | a is selected from the set of values b, c, d |
| [n:m] | Register bit field |
| .b | Byte mode selection |
| .d | Double-Word mode selection |
| .S | Shadow register select |
| .w | Word mode selection (default) |
| Acc | One of two accumulators {A, B} |
| AWB | Accumulator Write-Back Destination Address register ∈ {W13, [W13]+ = 2} |
| bit4 | 4-bit bit selection field (used in word-addressed instructions) ∈ {0...15} |
| C, DC, N, OV, Z | MCU Status bits: Carry, Digit Carry, Negative, Overflow, Sticky Zero |
| Expr | Absolute address, label or expression (resolved by the linker) |
| f | File register address ∈ {0x0000...0x1FFF} |
| lit1 | 1-bit unsigned literal ∈ {0,1} |
| lit4 | 4-bit unsigned literal ∈ {0...15} |
| lit5 | 5-bit unsigned literal ∈ {0...31} |
| lit8 | 8-bit unsigned literal ∈ {0...255} |
| lit10 | 10-bit unsigned literal ∈ {0...255} for Byte mode, {0:1023} for Word mode |
| lit14 | 14-bit unsigned literal ∈ {0...16384} |
| lit16 | 16-bit unsigned literal ∈ {0...65535} |
| lit23 | 23-bit unsigned literal ∈ {0...8388608}; LSb
must be ‘0’ |
| None | Field does not require an entry, can be blank |
| OA, OB, SA, SB | DSP Status bits: ACCA Overflow, ACCB Overflow, ACCA Saturate, ACCB Saturate |
| PC | Program Counter |
| Slit10 | 10-bit signed literal ∈ {-512...511} |
| Slit16 | 16-bit signed literal ∈ {-32768...32767} |
| Slit6 | 6-bit signed literal ∈ {-16...16} |
| Wb | Base W register ∈ {W0...W15} |
| Wd | Destination W register ∈ { Wd, [Wd], [Wd++], [Wd--], [++Wd], [--Wd] } |
| Wdo | Destination W register ∈ { Wnd, [Wnd], [Wnd++], [Wnd--], [++Wnd], [--Wnd], [Wnd+Wb] } |
| Wm,Wn | Dividend, Divisor Working register pair (direct addressing) |
| Wm*Wm | Multiplicand and Multiplier Working register pair for Square instructions ∈ {W4 * W4,W5 * W5,W6 * W6,W7 * W7} |
| Wm*Wn | Multiplicand and Multiplier Working register pair for DSP instructions ∈ {W4 * W5,W4 * W6,W4 * W7,W5 * W6,W5 * W7,W6 * W7} |
| Wn | One of 16 Working registers ∈ {W0...W15} |
| Wnd | One of 16 Destination Working registers ∈ {W0...W15} |
| Wns | One of 16 Source Working registers ∈ {W0...W15} |
| WREG | W0 (Working register used in file register instructions) |
| Ws | Source W register ∈ { Ws, [Ws], [Ws++], [Ws--], [++Ws], [--Ws] } |
| Wso | Source W register ∈ { Wns, [Wns], [Wns++], [Wns--], [++Wns], [--Wns], [Wns+Wb] } |
| Wx |
X Data Space Prefetch Address register for DSP instructions ∈ {[W8] + = 6, [W8] + = 4, [W8] + = 2, [W8], [W8] - = 6, [W8] - = 4, [W8] - = 2, [W9] + = 6, [W9] + = 4, [W9] + = 2, [W9], [W9] - = 6, [W9] - = 4, [W9] - = 2, [W9 + W12], none} |
| Wxd | X Data Space Prefetch Destination register for DSP instructions ∈ {W4...W7} |
| Wy |
Y Data Space Prefetch Address register for DSP instructions ∈ {[W10] + = 6, [W10] + = 4, [W10] + = 2, [W10], [W10] - = 6, [W10] - = 4, [W10] - = 2, [W11] + = 6, [W11] + = 4, [W11] + = 2, [W11], [W11] - = 6, [W11] - = 4, [W11] - = 2, [W11 + W12], none} |
| Wyd | Y Data Space Prefetch Destination register for DSP instructions ∈ {W4...W7} |
|
Note: In dsPIC33CDVL256MC506 devices, read and
Read-Modify-Write (RMW) operations on non-CPU Special Function Registers
require an additional cycle when compared to dsPIC30F, dsPIC33F, PIC24F and
PIC24H devices.
| |
|
Base Instr # | Assembly Mnemonic | Assembly Syntax | Description | # of Words | # of Cycles(1) | Status Flags Affected | |
|---|---|---|---|---|---|---|---|
| 1 | ADD | ADD | Acc | Add Accumulators | 1 | 1 | OA,OB,SA,SB |
ADD | f | f = f + WREG | 1 | 1 | C,DC,N,OV,Z | ||
ADD | f,WREG | WREG = f + WREG | 1 | 1 | C,DC,N,OV,Z | ||
ADD | #lit10,Wn | Wd = lit10 + Wd | 1 | 1 | C,DC,N,OV,Z | ||
ADD | Wb,Ws,Wd | Wd = Wb + Ws | 1 | 1 | C,DC,N,OV,Z | ||
ADD | Wb,#lit5,Wd | Wd = Wb + lit5 | 1 | 1 | C,DC,N,OV,Z | ||
ADD | Wso,#Slit4,Acc | 16-bit Signed Add to Accumulator | 1 | 1 | OA,OB,SA,SB | ||
| 2 | ADDC | ADDC | f | f = f + WREG + (C) | 1 | 1 | C,DC,N,OV,Z |
ADDC | f,WREG | WREG = f + WREG + (C) | 1 | 1 | C,DC,N,OV,Z | ||
ADDC | #lit10,Wn | Wd = lit10 + Wd + (C) | 1 | 1 | C,DC,N,OV,Z | ||
ADDC | Wb,Ws,Wd | Wd = Wb + Ws + (C) | 1 | 1 | C,DC,N,OV,Z | ||
ADDC | Wb,#lit5,Wd | Wd = Wb + lit5 + (C) | 1 | 1 | C,DC,N,OV,Z | ||
| 3 | AND | AND | f | f = f .AND. WREG | 1 | 1 | N,Z |
AND | f,WREG | WREG = f .AND. WREG | 1 | 1 | N,Z | ||
AND | #lit10,Wn | Wd = lit10 .AND. Wd | 1 | 1 | N,Z | ||
AND | Wb,Ws,Wd | Wd = Wb .AND. Ws | 1 | 1 | N,Z | ||
AND | Wb,#lit5,Wd | Wd = Wb .AND. lit5 | 1 | 1 | N,Z | ||
| 4 | ASR | ASR | f | f = Arithmetic Right Shift f | 1 | 1 | C,N,OV,Z |
ASR | f,WREG | WREG = Arithmetic Right Shift f | 1 | 1 | C,N,OV,Z | ||
ASR | Ws,Wd | Wd = Arithmetic Right Shift Ws | 1 | 1 | C,N,OV,Z | ||
ASR | Wb,Wns,Wnd | Wnd = Arithmetic Right Shift Wb by Wns | 1 | 1 | N,Z | ||
ASR | Wb,#lit5,Wnd | Wnd = Arithmetic Right Shift Wb by lit5 | 1 | 1 | N,Z | ||
| 5 | BCLR | BCLR | f,#bit4 | Bit Clear f | 1 | 1 | None |
BCLR | Ws,#bit4 | Bit Clear Ws | 1 | 1 | None | ||
| 6 | BFEXT | BFEXT | bit4,wid5,Ws,Wb | Bit Field Extract from Ws to Wb | 2 | 2 | None |
BFEXT | bit4,wid5,f,Wb | Bit Field Extract from f to Wb | 2 | 2 | None | ||
| 7 | BFINS | BFINS | bit4,wid5,Wb,Ws | Bit Field Insert from Wb into Ws | 2 | 2 | None |
BFINS | bit4,wid5,Wb,f | Bit Field Insert from Wb into f | 2 | 2 | None | ||
BFINS | bit4,wid5,lit8,Ws | Bit Field Insert from #lit8 to Ws | 2 | 2 | None | ||
| 8 | BOOTSWP | BOOTSWP | Swap the Active and Inactive Program Flash Space | 1 | 2 | None | |
| 9 | BRA | BRA | C,Expr | Branch if Carry | 1 | 1 (4)/1 | None |
BRA | GE,Expr | Branch if Greater Than or Equal | 1 | 1 (4)/1 | None | ||
BRA | GEU,Expr | Branch if unsigned Greater Than or Equal | 1 | 1 (4)/1 | None | ||
BRA | GT,Expr | Branch if Greater Than | 1 | 1 (4)/1 | None | ||
BRA | GTU,Expr | Branch if Unsigned Greater Than | 1 | 1 (4)/1 | None | ||
BRA | LE,Expr | Branch if Less Than or Equal | 1 | 1 (4)/1 | None | ||
BRA | LEU,Expr | Branch if Unsigned Less Than or Equal | 1 | 1 (4)/1 | None | ||
BRA | LT,Expr | Branch if Less Than | 1 | 1 (4)/1 | None | ||
BRA | LTU,Expr | Branch if Unsigned Less Than | 1 | 1 (4)/1 | None | ||
BRA | N,Expr | Branch if Negative | 1 | 1 (4)/1 | None | ||
BRA | NC,Expr | Branch if Not Carry | 1 | 1 (4)/1 | None | ||
BRA | NN,Expr | Branch if Not Negative | 1 | 1 (4)/1 | None | ||
BRA | NOV,Expr | Branch if Not Overflow | 1 | 1 (4)/1 | None | ||
BRA | NZ,Expr | Branch if Not Zero | 1 | 1 (4)/1 | None | ||
BRA | OA,Expr | Branch if Accumulator A Overflow | 1 | 1 (4)/1 | None | ||
BRA | OB,Expr | Branch if Accumulator B Overflow | 1 | 1 (4)/1 | None | ||
BRA | OV,Expr | Branch if Overflow | 1 | 1 (4)/1 | None | ||
BRA | SA,Expr | Branch if Accumulator A Saturated | 1 | 1 (4)/1 | None | ||
BRA | SB,Expr | Branch if Accumulator B Saturated | 1 | 1 (4)/1 | None | ||
BRA | Expr | Branch Unconditionally | 1 | 4/2 | None | ||
BRA | Z,Expr | Branch if Zero | 1 | 1 (4)/1 | None | ||
BRA | Wn | Computed Branch | 1 | 4 | None | ||
| 10 | BREAK | BREAK | Stop User Code Execution | 1 | 1 | None | |
| 11 | BSET | BSET | f,#bit4 | Bit Set f | 1 | 1 | None |
Ws,#bit4 | Bit Set Ws | 1 | 1 | None | |||
| 12 | BSW | BSW.C | Ws,Wb | Write C Bit to Ws[Wb] | 1 | 1 | None |
BSW.Z | Ws,Wb | Write Z Bit to Ws[Wb] | 1 | 1 | None | ||
| 13 | BTG | BTG | f,#bit4 | Bit Toggle f | 1 | 1 | None |
BTG | Ws,#bit4 | Bit Toggle Ws | 1 | 1 | None | ||
| 14 | BTSC | BTSC | f,#bit4 | Bit Test f, Skip if Clear | 1 | 1 (2 or 3) | None |
BTSC | Ws,#bit4 | Bit Test Ws, Skip if Clear | 1 | 1 (2 or 3) | None | ||
| 15 | BTSS | BTSS | f,#bit4 | Bit Test f, Skip if Set | 1 | 1 (2 or 3) | None |
BTSS | Ws,#bit4 | Bit Test Ws, Skip if Set | 1 | 1 (2 or 3) | None | ||
| 16 | BTST | BTST | f,#bit4 | Bit Test f | 1 | 1 | Z |
BTST.C | Ws,#bit4 | Bit Test Ws to C | 1 | 1 | C | ||
BTST.Z | Ws,#bit4 | Bit Test Ws to Z | 1 | 1 | Z | ||
BTST.C | Ws,Wb | Bit Test Ws[Wb] to C | 1 | 1 | C | ||
BTST.Z | Ws,Wb | Bit Test Ws[Wb] to Z | 1 | 1 | Z | ||
| 17 | BTSTS | BTSTS | f,#bit4 | Bit Test then Set f | 1 | 1 | Z |
BTSTS.C | Ws,#bit4 | Bit Test Ws to C, then Set | 1 | 1 | C | ||
BTSTS.Z | Ws,#bit4 | Bit Test Ws to Z, then Set | 1 | 1 | Z | ||
| 18 | CALL | CALL | lit23 | Call Subroutine | 2 | 4/(2) | SFA |
CALL | Wn | Call Indirect Subroutine | 1 | 4(2) | SFA | ||
CALL.L | Wn | Call Indirect Subroutine (long address) | 1 | 4(2) | SFA | ||
| 19 | CLR | CLR | f | f = 0x0000 | 1 | 1 | None |
CLR | WREG | WREG = 0x0000 | 1 | 1 | None | ||
CLR | Ws | Ws = 0x0000 | 1 | 1 | None | ||
CLR | Acc,Wx,Wxd,Wy,Wyd,AWB | Clear Accumulator | 1 | 1 | OA,OB,SA,SB | ||
| 20 | CLRWDT | CLRWDT | Clear Watchdog Timer | 1 | 1 | WDTO,Sleep | |
| 21 | COM | COM | f | f = f | 1 | 1 | N,Z |
COM | f,WREG | WREG = f | 1 | 1 | N,Z | ||
COM | Ws,Wd | Wd = Ws | 1 | 1 | N,Z | ||
| 22 | CP | CP | f | Compare f with WREG | 1 | 1 | C,DC,N,OV,Z |
CP | Wb,#lit8 | Compare Wb with lit8 | 1 | 1 | C,DC,N,OV,Z | ||
CP | Wb,Ws | Compare Wb with Ws (Wb – Ws) | 1 | 1 | C,DC,N,OV,Z | ||
| 23 | CP0 | CP0 | f | Compare f with 0x0000 | 1 | 1 | C,DC,N,OV,Z |
CP0 | Ws | Compare Ws with 0x0000 | 1 | 1 | C,DC,N,OV,Z | ||
| 24 | CPB | CPB | f | Compare f with WREG, with Borrow | 1 | 1 | C,DC,N,OV,Z |
CPB | Wb,#lit8 | Compare Wb with lit8, with Borrow | 1 | 1 | C,DC,N,OV,Z | ||
CPB | Wb,Ws | Compare Wb with Ws, with Borrow (Wb – Ws – C) | 1 | 1 | C,DC,N,OV,Z | ||
| 25 | CPSEQ | CPSEQ | Wb,Wn | Compare Wb with Wn, Skip if = | 1 | 1 (2 or 3) | None |
CPBEQ | CPBEQ | Wb,Wn,Expr | Compare Wb with Wn, Branch if = | 1 | 1 (5) | None | |
| 26 | CPSGT | CPSGT | Wb,Wn | Compare Wb with Wn, Skip if > | 1 | 1 (2 or 3) | None |
CPBGT | CPBGT | Wb,Wn,Expr | Compare Wb with Wn, Branch if > | 1 | 1 (5) | None | |
| 27 | CPSLT | CPSLT | Wb,Wn | Compare Wb with Wn, Skip if < | 1 | 1 (2 or 3) | None |
CPBLT | Wb,Wn,Expr | Compare Wb with Wn, Branch if < | 1 | 1 (5) | None | ||
| 28 | CPSNE | CPSNE | Wb,Wn | Compare Wb with Wn, Skip if ≠ | 1 | 1 (2 or 3) | None |
CPBNE | Wb,Wn,Expr | Compare Wb with Wn, Branch if ≠ | 1 | 1 (5) | None | ||
| 29 | CTXTSWP | CTXTSWP | #1it3 | Switch CPU Register Context to Context Defined by lit3 | 1 | 2 | None |
| 30 | CTXTSWP | CTXTSWP | Wn | Switch CPU Register Context to Context Defined by Wn | 1 | 2 | None |
| 31 | DAW.B | DAW.B | Wn | Wn = Decimal Adjust Wn | 1 | 1 | C |
| 32 | DEC | DEC | f | f = f – 1 | 1 | 1 | C,DC,N,OV,Z |
DEC | f,WREG | WREG = f – 1 | 1 | 1 | C,DC,N,OV,Z | ||
DEC | Ws,Wd | Wd = Ws – 1 | 1 | 1 | C,DC,N,OV,Z | ||
| 33 | DEC2 | DEC2 | f | f = f – 2 | 1 | 1 | C,DC,N,OV,Z |
DEC2 | f,WREG | WREG = f – 2 | 1 | 1 | C,DC,N,OV,Z | ||
DEC2 | Ws,Wd | Wd = Ws – 2 | 1 | 1 | C,DC,N,OV,Z | ||
| 34 | DISI | DISI | #lit14 | Disable Interrupts for k Instruction Cycles | 1 | 1 | None |
| 35 | DIVF(2) | DIVF | Wm,Wn | Signed 16/16-Bit Fractional Divide | 1 | 18/6 | N,Z,C,OV |
| 36 | DIV.S(2) | DIV.S | Wm,Wn | Signed 16/16-Bit Integer Divide | 1 | 18/6 | N,Z,C,OV |
DIV.SD | Wm,Wn | Signed 32/16-Bit Integer Divide | 1 | 18/6 | N,Z,C,OV | ||
| 37 | DIV.U(2) | DIV.U | Wm,Wn | Unsigned 16/16-Bit Integer Divide | 1 | 18/6 | N,Z,C,OV |
DIV.UD | Wm,Wn | Unsigned 32/16-Bit Integer Divide | 1 | 18/6 | N,Z,C,OV | ||
| 38 | DIVF2(2) | DIVF2 | Wm,Wn | Signed 16/16-Bit Fractional Divide (W1:W0 preserved) | 1 | 6 | N,Z,C,OV |
| 39 | DIV2.S(3) | DIV2.S | Wm,Wn | Signed 16/16-Bit Integer Divide (W1:W0 preserved) | 1 | 6 | N,Z,C,OV |
DIV2.SD | Wm,Wn | Signed 32/16-Bit Integer Divide (W1:W0 preserved) | 1 | 6 | N,Z,C,OV | ||
| 40 | DIV2.U(2) | DIV2.U | Wm,Wn | Unsigned 16/16-Bit Integer Divide (W1:W0 preserved) | 1 | 6 | N,Z,C,OV |
DIV2.UD | Wm,Wn | Unsigned 32/16-Bit Integer Divide (W1:W0 preserved) | 1 | 6 | N,Z,C,OV | ||
| 41 | DO | DO | #lit15,Expr | Do Code to PC + Expr, lit15 + 1 Times | 2 | 2 | None |
DO | Wn,Expr | Do code to PC + Expr, (Wn) + 1 Times | 2 | 2 | None | ||
| 42 | ED | ED | Wm*Wm,Acc,Wx,Wy,Wxd | Euclidean Distance (no accumulate) | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
| 43 | EDAC | EDAC | Wm*Wm,Acc,Wx,Wy,Wxd | Euclidean Distance | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
| 44 | EXCH | EXCH | Wns,Wnd | Swap Wns with Wnd | 1 | 1 | None |
| 46 | FBCL | FBCL | Ws,Wnd | Find Bit Change from Left (MSb) Side | 1 | 1 | C |
| 47 | FF1L | FF1L | Ws,Wnd | Find First One from Left (MSb) Side | 1 | 1 | C |
| 48 | FF1R | FF1R | Ws,Wnd | Find First One from Right (LSb) Side | 1 | 1 | C |
| 49 | FLIM | FLIM | Wb, Ws | Force Data (Upper and Lower) Range Limit without Limit Excess Result | 1 | 1 | N,Z,OV |
FLIM.V | Wb, Ws, Wd | Force Data (Upper and Lower) Range Limit with Limit Excess Result | 1 | 1 | N,Z,OV | ||
| 50 | GOTO | GOTO | Expr | Go to Address | 2 | 4/2 | None |
GOTO | Wn | Go to Indirect | 1 | 4/2 | None | ||
GOTO.L | Wn | Go to Indirect (long address) | 1 | 4/2 | None | ||
| 51 | INC | INC | f | f = f + 1 | 1 | 1 | C,DC,N,OV,Z |
INC | f,WREG | WREG = f + 1 | 1 | 1 | C,DC,N,OV,Z | ||
INC | Ws,Wd | Wd = Ws + 1 | 1 | 1 | C,DC,N,OV,Z | ||
| 52 | INC2 | INC2 | f | f = f + 2 | 1 | 1 | C,DC,N,OV,Z |
INC2 | f,WREG | WREG = f + 2 | 1 | 1 | C,DC,N,OV,Z | ||
INC2 | Ws,Wd | Wd = Ws + 2 | 1 | 1 | C,DC,N,OV,Z | ||
| 53 | IOR | IOR | f | f = f .IOR. WREG | 1 | 1 | N,Z |
IOR | f,WREG | WREG = f .IOR. WREG | 1 | 1 | N,Z | ||
IOR | #lit10,Wn | Wd = lit10 .IOR. Wd | 1 | 1 | N,Z | ||
IOR | Wb,Ws,Wd | Wd = Wb .IOR. Ws | 1 | 1 | N,Z | ||
IOR | Wb,#lit5,Wd | Wd = Wb .IOR. lit5 | 1 | 1 | N,Z | ||
| 54 | LAC | LAC | Wso,#Slit4,Acc | Load Accumulator | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
LAC.D | Wso, #Slit4, Acc | Load Accumulator Double | 1 | 2 | OA,SA,OB,SB | ||
| 56 | LNK | LNK | #lit14 | Link Frame Pointer | 1 | 1 | SFA |
| 57 | LSR | LSR | f | f = Logical Right Shift f | 1 | 1 | C,N,OV,Z |
LSR | f,WREG | WREG = Logical Right Shift f | 1 | 1 | C,N,OV,Z | ||
LSR | Ws,Wd | Wd = Logical Right Shift Ws | 1 | 1 | C,N,OV,Z | ||
LSR | Wb,Wns,Wnd | Wnd = Logical Right Shift Wb by Wns | 1 | 1 | N,Z | ||
LSR | Wb,#lit5,Wnd | Wnd = Logical Right Shift Wb by lit5 | 1 | 1 | N,Z | ||
| 58 | MAC | MAC | Wm*Wn,Acc,Wx,Wxd,
| Multiply and Accumulate | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
MAC | Wm*Wm,Acc,Wx,Wxd,
| Square and Accumulate | 1 | 1 | OA,OB,OAB, SA,SB,SAB | ||
| 59 | MAX | MAX | Acc | Force Data Maximum Range Limit | 1 | 1 | N,OV,Z |
MAX.V | Acc, Wnd | Force Data Maximum Range Limit with Result | 1 | 1 | N,OV,Z | ||
| 60 | MIN | MIN | Acc | If Accumulator A Less than B Load Accumulator with B or vice versa | 1 | 1 | N,OV,Z |
MIN.V | Acc, Wd | If Accumulator A Less than B Accumulator Force Minimum Data Range Limit with Limit Excess Result | 1 | 1 | N,OV,Z | ||
MINZ | Acc | Accumulator Force Minimum Data Range Limit | 1 | 1 | N,OV,Z | ||
MINZ.V | Acc, Wd | Accumulator Force Minimum Data Range Limit with Limit Excess Result | 1 | 1 | N,OV,Z | ||
| 61 | MOV | MOV | f,Wn | Move f to Wn | 1 | 1 | None |
MOV | f | Move f to f | 1 | 1 | None | ||
MOV | f,WREG | Move f to WREG | 1 | 1 | None | ||
MOV | #lit16,Wn | Move 16-Bit Literal to Wn | 1 | 1 | None | ||
MOV.b | #lit8,Wn | Move 8-Bit Literal to Wn | 1 | 1 | None | ||
MOV | Wn,f | Move Wn to f | 1 | 1 | None | ||
MOV | Wso,Wdo | Move Ws to Wd | 1 | 1 | None | ||
MOV | WREG,f | Move WREG to f | 1 | 1 | None | ||
MOV.D
Wns,Wd | Move Double from W(ns):W(ns + 1) to Wd | 1 | 2 | None | |||
MOV.D
Ws,Wnd | Move Double from Ws to W(nd + 1):W(nd) | 1 | 2 | None | |||
| 62 | MOVPAG | MOVPAG | #lit10,DSRPAG | Move 10-Bit Literal to DSRPAG | 1 | 1 | None |
MOVPAG | #lit8,TBLPAG | Move 8-Bit Literal to TBLPAG | 1 | 1 | None | ||
MOVPAG | Ws, DSRPAG | Move Ws[9:0] to DSRPAG | 1 | 1 | None | ||
MOVPAG | Ws, TBLPAG | Move Ws[7:0] to TBLPAG | 1 | 1 | None | ||
| 64 | MOVSAC | MOVSAC | Acc,Wx,Wxd,Wy,Wyd,AWB | Prefetch and Store Accumulator | 1 | 1 | None |
| 65 | MPY | MPY
Wm*Wn,Acc,Wx,Wxd,Wy,Wyd | Multiply Wm by Wn to Accumulator | 1 | 1 | OA,OB,OAB, SA,SB,SAB | |
MPY
Wm*Wm,Acc,Wx,Wxd,Wy,Wyd | Square Wm to Accumulator | 1 | 1 | OA,OB,OAB, SA,SB,SAB | |||
| 66 | MPY.N | MPY.N
Wm*Wn,Acc,Wx,Wxd,Wy,Wyd | -(Multiply Wm by Wn) to Accumulator | 1 | 1 | None | |
| 67 | MSC | MSC | Wm*Wm,Acc,Wx,Wxd,
| Multiply and Subtract from Accumulator | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
| 68 | MUL | MUL.SS | Wb,Ws,Wnd | {Wnd + 1, Wnd} = Signed(Wb) * Signed(Ws) | 1 | 1 | None |
MUL.SS | Wb,Ws,Acc | Accumulator = Signed(Wb) * Signed(Ws) | 1 | 1 | None | ||
MUL.SU | Wb,Ws,Wnd | {Wnd + 1, Wnd} = Signed(Wb) * Unsigned(Ws) | 1 | 1 | None | ||
MUL.SU | Wb,Ws,Acc | Accumulator = Signed(Wb) * Unsigned(Ws) | 1 | 1 | None | ||
MUL.SU | Wb,#lit5,Acc | Accumulator = Signed(Wb) * Unsigned(lit5) | 1 | 1 | None | ||
MUL.US | Wb,Ws,Wnd | {Wnd + 1, Wnd} = Unsigned(Wb) * Signed(Ws) | 1 | 1 | None | ||
MUL.US | Wb,Ws,Acc | Accumulator = Unsigned(Wb) * Signed(Ws) | 1 | 1 | None | ||
MUL.UU | Wb,Ws,Wnd | {Wnd + 1, Wnd} = Unsigned(Wb) * Unsigned(Ws) | 1 | 1 | None | ||
MUL.UU | Wb,#lit5,Acc | Accumulator = Unsigned(Wb) * Unsigned(lit5) | 1 | 1 | None | ||
MUL.UU | Wb,Ws,Acc | Accumulator = Unsigned(Wb) * Unsigned(Ws) | 1 | 1 | None | ||
MULW.SS | Wb,Ws,Wnd | Wnd = Signed(Wb) * Signed(Ws) | 1 | 1 | None | ||
MULW.SU | Wb,Ws,Wnd | Wnd = Signed(Wb) * Unsigned(Ws) | 1 | 1 | None | ||
MULW.US | Wb,Ws,Wnd | Wnd = Unsigned(Wb) * Signed(Ws) | 1 | 1 | None | ||
MULW.UU | Wb,Ws,Wnd | Wnd = Unsigned(Wb) * Unsigned(Ws) | 1 | 1 | None | ||
MUL.SU | Wb,#lit5,Wnd | {Wnd + 1, Wnd} = Signed(Wb) * Unsigned(lit5) | 1 | 1 | None | ||
MUL.SU | Wb,#lit5,Wnd | Wnd = Signed(Wb) * Unsigned(lit5) | 1 | 1 | None | ||
MUL.UU | Wb,#lit5,Wnd | {Wnd + 1, Wnd} = Unsigned(Wb) * Unsigned(lit5) | 1 | 1 | None | ||
MUL.UU | Wb,#lit5,Wnd | Wnd = Unsigned(Wb) * Unsigned(lit5) | 1 | 1 | None | ||
MUL | f | W3:W2 = f * WREG | 1 | 1 | None | ||
| 69 | NEG | NEG | Acc | Negate Accumulator | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
NEG | f | f = f + 1 | 1 | 1 | C,DC,N,OV,Z | ||
NEG | f,WREG | WREG = f + 1 | 1 | 1 | C,DC,N,OV,Z | ||
NEG | Ws,Wd | Wd = Ws + 1 | 1 | 1 | C,DC,N,OV,Z | ||
| 70 | NOP | NOP | No Operation | 1 | 1 | None | |
NOPR | No Operation | 1 | 1 | None | |||
| 71 | NORM | NORM | Acc, Wd | Normalize Accumulator | 1 | 1 | N,OV,Z |
| 72 | POP | POP | f | Pop f from Top-of-Stack (TOS) | 1 | 1 | None |
POP | Wdo | Pop from Top-of-Stack (TOS) to Wdo | 1 | 1 | None | ||
POP.D | Wnd | Pop from Top-of-Stack (TOS) to W(nd):W(nd + 1) | 1 | 2 | None | ||
POP.S | Pop Shadow Registers | 1 | 1 | All | |||
| 73 | PUSH | PUSH | | Push f to Top-of-Stack (TOS) | 1 | 1 | None |
PUSH | Wso | Push Wso to Top-of-Stack (TOS) | 1 | 1 | None | ||
PUSH.D | Wns | Push W(ns):W(ns + 1) to Top-of-Stack (TOS) | 1 | 2 | None | ||
PUSH.S | Push Shadow Registers | 1 | 1 | None | |||
| 74 | PWRSAV | PWRSAV
#lit1 | Go into Sleep or Idle mode | 1 | 1 | WDTO,Sleep | |
| 75 | RCALL | RCALL | Expr | Relative Call | 1 | 4/2 (2) | SFA |
RCALL | Wn | Computed Call | 1 | 4/2 (2) | SFA | ||
| 76 | REPEAT | REPEAT | #lit15 | Repeat Next Instruction lit15 + 1 Times | 1 | 1 | None |
REPEAT | Wn | Repeat Next Instruction (Wn) + 1 Times | 1 | 1 | None | ||
| 77 | RESET | RESET | Software Device Reset | 1 | 1 | None | |
| 78 | RETFIE | RETFIE | Return from Interrupt | 1 | 6 (5)/3 (2) | SFA | |
| 79 | RETLW | RETLW | #lit10,Wn | Return with Literal in Wn | 1 | 6 (5)/3 (2) | SFA |
| 80 | RETURN | RETURN | Return from Subroutine | 1 | 6 (5)/3 (2) | SFA | |
| 81 | RLC | RLC | f | f = Rotate Left through Carry f | 1 | 1 | C,N,Z |
RLC | f,WREG | WREG = Rotate Left through Carry f | 1 | 1 | C,N,Z | ||
RLC | Ws,Wd | Wd = Rotate Left through Carry Ws | 1 | 1 | C,N,Z | ||
| 82 | RLNC | RLNC | f | f = Rotate Left (No Carry) f | 1 | 1 | N,Z |
RLNC | f,WREG | WREG = Rotate Left (No Carry) f | 1 | 1 | N,Z | ||
RLNC | Ws,Wd | Wd = Rotate Left (No Carry) Ws | 1 | 1 | N,Z | ||
| 83 | RRC | RRC | f | f = Rotate Right through Carry f | 1 | 1 | C,N,Z |
RRC | f,WREG | WREG = Rotate Right through Carry f | 1 | 1 | C,N,Z | ||
RRC | Ws,Wd | Wd = Rotate Right through Carry Ws | 1 | 1 | C,N,Z | ||
| 84 | RRNC | RRNC | f | f = Rotate Right (No Carry) f | 1 | 1 | N,Z |
RRNC | f,WREG | WREG = Rotate Right (No Carry) f | 1 | 1 | N,Z | ||
RRNC | Ws,Wd | Wd = Rotate Right (No Carry) Ws | 1 | 1 | N,Z | ||
| 85 | SAC | SAC | Acc,#Slit4,Wdo | Store Accumulator | 1 | 1 | None |
SAC.R | Acc,#Slit4,Wdo | Store Rounded Accumulator | 1 | 1 | None | ||
SAC.D | #Slit4, Wdo | Store Accumulator Double | 1 | 1 | None | ||
| 86 | SE | SE | Ws,Wnd | Wnd = Sign-Extended Ws | 1 | 1 | C,N,Z |
| 87 | SETM | SETM | f | f = 0xFFFF | 1 | 1 | None |
SETM | WREG | WREG = 0xFFFF | 1 | 1 | None | ||
SETM | Ws | Ws = 0xFFFF | 1 | 1 | None | ||
| 88 | SFTAC | SFTAC | Acc,Wn | Arithmetic Shift Accumulator by (Wn) | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
SFTAC | Acc,#Slit6 | Arithmetic Shift Accumulator by Slit6 | 1 | 1 | OA,OB,OAB, SA,SB,SAB | ||
| 89 | SL | SL | f | f = Left Shift f | 1 | 1 | C,N,OV,Z |
SL | f,WREG | WREG = Left Shift f | 1 | 1 | C,N,OV,Z | ||
SL | Ws,Wd | Wd = Left Shift Ws | 1 | 1 | C,N,OV,Z | ||
SL | Wb,Wns,Wnd | Wnd = Left Shift Wb by Wns | 1 | 1 | N,Z | ||
SL | Wb,#lit5,Wnd | Wnd = Left Shift Wb by lit5 | 1 | 1 | N,Z | ||
| 91 | SUB | SUB | Acc | Subtract Accumulators | 1 | 1 | OA,OB,OAB, SA,SB,SAB |
SUB | f | f = f – WREG | 1 | 1 | C,DC,N,OV,Z | ||
SUB | f,WREG | WREG = f – WREG | 1 | 1 | C,DC,N,OV,Z | ||
SUB | #lit10,Wn | Wn = Wn – lit10 | 1 | 1 | C,DC,N,OV,Z | ||
SUB | Wb,Ws,Wd | Wd = Wb – Ws | 1 | 1 | C,DC,N,OV,Z | ||
SUB | Wb,#lit5,Wd | Wd = Wb – lit5 | 1 | 1 | C,DC,N,OV,Z | ||
| 92 | SUBB | SUBB | f | f = f – WREG – (C) | 1 | 1 | C,DC,N,OV,Z |
SUBB | f,WREG | WREG = f – WREG – (C) | 1 | 1 | C,DC,N,OV,Z | ||
SUBB | #lit10,Wn | Wn = Wn – lit10 – (C) | 1 | 1 | C,DC,N,OV,Z | ||
SUBB | Wb,Ws,Wd | Wd = Wb – Ws – (C) | 1 | 1 | C,DC,N,OV,Z | ||
SUBB | Wb,#lit5,Wd | Wd = Wb – lit5 – (C) | 1 | 1 | C,DC,N,OV,Z | ||
| 93 | SUBR | SUBR | f | f = WREG – f | 1 | 1 | C,DC,N,OV,Z |
SUBR | f,WREG | WREG = WREG – f | 1 | 1 | C,DC,N,OV,Z | ||
SUBR | Wb,Ws,Wd | Wd = Ws – Wb | 1 | 1 | C,DC,N,OV,Z | ||
SUBR | Wb,#lit5,Wd | Wd = lit5 – Wb | 1 | 1 | C,DC,N,OV,Z | ||
| 94 | SUBBR | SUBBR | f | f = WREG – f – (C) | 1 | 1 | C,DC,N,OV,Z |
SUBBR | f,WREG | WREG = WREG – f – (C) | 1 | 1 | C,DC,N,OV,Z | ||
SUBBR | Wb,Ws,Wd | Wd = Ws – Wb – (C) | 1 | 1 | C,DC,N,OV,Z | ||
SUBBR | Wb,#lit5,Wd | Wd = lit5 – Wb – (C) | 1 | 1 | C,DC,N,OV,Z | ||
| 95 | SWAP | SWAP.b | Wn | Wn = Nibble Swap Wn | 1 | 1 | None |
SWAP | Wn | Wn = Byte Swap Wn | 1 | 1 | None | ||
| 96 | TBLRDH | TBLRDH | Ws,Wd | Read Prog[23:16] to Wd[7:0] | 1 | 5/3 (2) | None |
| 97 | TBLRDL | TBLRDL | Ws,Wd | Read Prog[15:0] to Wd | 1 | 5/3 (2) | None |
| 98 | TBLWTH | TBLWTH | Ws,Wd | Write Ws[7:0] to Prog[23:16] | 1 | 2 | None |
| 99 | TBLWTL | TBLWTL | Ws,Wd | Write Ws to Prog[15:0] | 1 | 2 | None |
| 101 | ULNK | ULNK | Unlink Frame Pointer | 1 | 1 | SFA | |
| 104 | XOR | XOR | f | f = f .XOR. WREG | 1 | 1 | N,Z |
XOR | f,WREG | WREG = f .XOR. WREG | 1 | 1 | N,Z | ||
XOR | #lit10,Wn | Wd = lit10 .XOR. Wd | 1 | 1 | N,Z | ||
XOR | Wb,Ws,Wd | Wd = Wb .XOR. Ws | 1 | 1 | N,Z | ||
XOR | Wb,#lit5,Wd | Wd = Wb .XOR. lit5 | 1 | 1 | N,Z | ||
| 105 | ZE | ZE | Ws,Wnd | Wnd = Zero-Extend Ws | 1 | 1 | C,Z,N |
|
Note:
| |||||||