1.3.6 DDR Interface

The DDR_Interface block demonstrates Debug DDR IO Margin feature in SmartDebug. Select the Debug DDR Memory option in the main SmartDebug window. Debug DDR Memory is available only for DDR3/DDR4/LPDDR3 memory configurations on PolarFire devices. This option is not visible when DDR memory is not used in the design.

Important: For detailed information on DDR Debug, see SmartDebug User Guide.
Figure 1-4. DDR Interface Overall Blocks