4.3 PIC32MX Power Requirements
Devices in the PIC32MX family are dual voltage supply designs. There is one supply for
the core and another for peripherals and I/O pins. All devices contain an on-chip
regulator for the lower voltage core supply to eliminate the need for an additional
external regulator. There are three implementations of the on board regulator:
- The first version has an internal regulator that can be disabled using the ENVREG pin. When disabled, an external power supply must be used to power the core. If enabled, a low-ESR filter capacitor must be connected to the VCAP pin, see Figure 4-2.
- The second version has an internal regulator that cannot be disabled. A low-ESR filter capacitor must always be connected to the VCAP pin.
- The third version has an internal regulator that cannot be disabled and does not require a filter capacitor
Refer to “AC/DC Characteristics and Timing Requirements” and the “Electrical Characteristics” chapter in the specific device data sheet for the power requirements of the device.
Note:
- These are typical operating voltages. Refer to the AC/DC Characteristics and Timing Requirements for the full operating ranges of VDD and VCAP.
- Regulator Enabled and Regulator Disabled mode are not available on all devices. Refer to the specific device data sheet to determine availability.