1.1.4.2 DRV_METROLOGY_Reinitialize Function
SYS_MODULE_OBJ DRV_METROLOGY_Reinitialize (
SYS_MODULE_INIT * init
);SummaryRe-initializes the metrology driver according to the init parameter.
DescriptionThis routine re-initializes the metrology driver resetting the Coprocessor and its peripherals and re-loading the metrology library application on Core 1 from scratch. The initialization data is specified by the init parameter. It is a single instance driver.
PreconditionThe low-level board initialization must have been completed and the module's initialization function must have been called before the system.
Parameters| Param | Description |
|---|---|
| init | Pointer to the init data structure containing any data necessary to initialize the driver. |
If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
Example SYS_MODULE_OBJ sysObjDrvMet;
extern uint8_t met_bin_start;
extern uint8_t met_bin_end;
DRV_METROLOGY_INIT drvMetrologyInitData = {
.regBaseAddress = DRV_METROLOGY_REG_BASE_ADDRESS,
.binStartAddress = (uint32_t)&met_bin_start,
.binEndAddress = (uint32_t)&met_bin_end,
};
sysObjDrvMet = DRV_METROLOGY_Reinitialize((SYS_MODULE_INIT *)&drvMetrologyInitData);RemarksDRV_METROLOGY_Initialize routine has to be called at some point before this routine is called.