1.1.4.26 DRV_METROLOGY_GetCalibrationReferences Function
C
DRV_METROLOGY_CALIBRATION_REFS * DRV_METROLOGY_GetCalibrationReferences (void);SummaryGets the pointer to the calibration references to be used in the internal calibration process of the metrology library.
DescriptionThese internal calibration values set the target values to be measured, and will be the target on next calibration process when triggered.
The same pointed structure will include the result of the calibration process when finished, so it can be checked by the main application.
ParametersNone.
ReturnsPointer to the calibration references to be used in the next calibration process.
Example void APP_METROLOGY_StartCalibration(APP_METROLOGY_CALIBRATION * calibration)
{
DRV_METROLOGY_CALIBRATION_REFS * pCalibrationRefs;
pCalibrationRefs = DRV_METROLOGY_GetCalibrationReferences();
pCalibrationRefs->va = 220;
pCalibrationRefs->ia = 30;
pCalibrationRefs->aa = 60;
pCalibrationRefs->calMask.magnitudeVa = 1;
pCalibrationRefs->calMask.magnitudeIa = 1;
pCalibrationRefs->calMask.anglePhaseA = 1;
app_metrologyData.state = APP_METROLOGY_STATE_CHECK_CALIBRATION;
DRV_METROLOGY_StartCalibration();
}RemarksNone.