3.4.8.3.1 Set Up the Warrant File
Before starting the key export, make sure to copy the HSM module warrant file from nCipher into
the Tools directory. This file contains a cryptogram that
identifies the origin of the HSM module. The file name follows
the format warrant‑[ESN].txt, where ESN is the module
serial number that can be printed using the
nfkminfo utility. The following is
an example of the warrant file copied into the Tools
directory:
C:\Microsemi\Tools\warrant-586F-B963-9146.txt