3.4.8.3.3 Export Public Key for Verifying Signature
Enter the following command to export:
ExportSeeKey.bat g4cu-seessk-<U_UUID>
This file is placed in the current directory (Tools, in this case). The following figure shows a sample output.
Once exported, these files must be imported into the following HSMs, depending on your particular flow:
- This U-HSM server, to enable M-HSM function if the M-HSM function is used.
- M-HSM(s) that are to execute jobs generated by this U-HSM server, if used.
- Microchip Manufacturing (MFG) HSM: Required. See section Key Exchange with Microchip.
- Microchip IHP, if used.