2.1.3.4.2 Verilog Task-Based Flag Assertion
(Ask a Question)The LSRAM simulation model feature allows you to control the ECC error flags through your environment by using Verilog tasks. While using this feature, ensure that you have not activated the probability based ECC error flag simulation as described in Probability-Based ECC Flag Assertion.
The Verilog task-based simulation can be performed on any of your
projects without regenerating any of the cores. To use this feature, you must enter the
address for which you want an ECC flag along with data mask bits, which decide to assert
either SB_CORRECT or DB_DETECT flags in the
user_ecc_wrapper.v, and include the
generated_ecc_wrapper.v file in the active test bench.
To enable or disable the ECC error flags feature in the simulation
model, execute the
ecc_err_inject_inst.enable_ecc_err_inject(1’b<user-input>)
task with the values described in the following table:
| User-Input | Result |
|---|---|
1 | The ECC error flag feature is enabled. |
0 | The ECC error flag feature is disabled
(default). Note: If this feature is
disabled, the simulation model does not respond to other related
tasks. |
To control the ECC error flags for a single address, execute the
inject_single_addr_ecc_errors(<address>,<data_mask>)
task with the values described in the following table:
| Argument | Description |
|---|---|
address | The user address to which the simulation model must drive the ECC error flags. |
data_mask | The data mask bits that decide single or dual bit ECC flag. |
During read operation, when the read address is equal to the
<address> specified in this task, the following conditional
results are achieved:
| Result... | if... |
|---|---|
The SB_CORRECT error
flag is asserted to 1 and read data remains
unchanged. | The specified
<data_mask> has only one non-zero
bit. |
The DB_DETECT and
SB_CORRECT error flags are asserted to
1 and the read data bit is negated where
<data_mask> bit is 1.Note: For some configurations, even though
you provide the Data Mask bits > 1, it may still turn into SB
flag only and not DB flag, as each of those Data mask bits belong to
different physical instance block. | The specified
<data_mask> has more than one non-zero
bit. |