2.1.3.4.3 Simulation Flow Example
(Ask a Question)The following is an example to simulate your design with the ECC error flag feature enabled.
- Enter all ECC related Verilog tasks
as per the Logical Address in the
user_ecc_wrapper.vfile in the following format.sd_0.PF_TPSRAM_C0.ecc_err_inject_inst.enable_ecc_err_inject(1'b1); sd_0.PF_TPSRAM_C0.inject_single_addr_ecc_errors(m'hLA1,n'hDM_LA1); ...Table 2-15. ECC Include File Format Format Description sd_0Design instance name in the testbench PF_TPSRAM_C0Logical instance name of PolarFire Two-Port Large SRAM in the design mSize of the logical address LA1Logical address nSize of the data mask DM_LA1Data mask bits for the logical address Important: Ensure that you provide the accurate hierarchy up to the LSRAM instance before populating theecc_err_inject_inst.enable_ecc_err_injectandinject_single_addr_ecc_errorstasks in theuser_ecc_wrapper.vfile.The following is an example with the logical configuration of depth set to
4096, width set to20ofPF_TPSRAMin the designsd_0with logical instancePF_TPSRAM_C0.initial begin tb.sd_0.PF_TPSRAM_C0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0.inject_single_addr_ecc_errors(12'h100 ,20'h00002); tb.sd_0.PF_TPSRAM_C0.inject_single_addr_ecc_errors(12'h1a0 ,20'h00003); tb.sd_0.PF_TPSRAM_C0.inject_single_addr_ecc_errors(12'h1ff ,20'h00004); end - Download the PolarFire_ecc_include_file_gen.py Python script file to your computer.
- Extract the contents of the
.zipfile to any location on the computer. - Use any standard Python executor and
change the directory to the location where the script is extracted and execute the
PolarFire_ecc_include_file_gen.pypython script with the following arguments.python PolarFire_ecc_include_file_gen.py <libero_project_location> <user_ecc_wrapper.v>Example 1: In the following example, the
user_ecc_wrapper.vfile and the script file are placed in the same location as that of the Libero project.python PolarFire_ecc_include_file_gen.py . .Example 2: In the following example, the
user_ecc_wrapper.vfile is located inside the stimulus folder under the Libero project folder, which is located in the pathD:/user/test_ecc.python PolarFire_ecc_include_file_gen.py D:/user/test_ecc D:/user/test_ecc/stimulusAfter successful execution of the script, the
generated_ecc_wrapper.vfile is generated with the physical block instance name embedded in the hierarchical path and both Address and Data Mask breakdown, as shown in the following example:initial begin //tb.sd_0.PF_TPSRAM_C0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R0C0.u0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R1C0.u0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R2C0.u0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R3C0.u0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R4C0.u0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R5C0.u0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R6C0.u0.enable_ecc_err_inject(1'b1); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R7C0.u0.enable_ecc_err_inject(1'b1); //tb.sd_0.PF_TPSRAM_C0.inject_single_addr_ecc_errors(12'h100 ,20'h00002); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R0C0.u0.inject_single_addr_ecc_errors(9'h100,33'h2); //tb.sd_0.PF_TPSRAM_C0.inject_single_addr_ecc_errors(12'h1a0 ,20'h00003); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R0C0.u0.inject_single_addr_ecc_errors(9'h1a0,33'h3); //tb.sd_0.PF_TPSRAM_C0.inject_single_addr_ecc_errors(12'h1ff ,20'h00004); tb.sd_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_0.PF_TPSRAM_C0_PF_TPSRAM_C0_0_PF_TPSRAM_R0C0.u0.inject_single_addr_ecc_errors(9'h1ff,33'h4); end - Run the Simulation using any one of the following methods, after the
generated_ecc_wrapper.vfile is generated.- Without modifying the
testbench:Compile the
generated_user_ecc_wrapper.vfile using therun.dofile as shown in the following figure.Figure 2-21. run.doFile - Modifying the
testbench:Directly place the
generated_ecc_wrapper.vfile at the same location as that of the testbench and include the file after instantiating the design under test as follows or provide the absolute path of thegenerated_ecc_wrapper.vfile:`include “generated_ecc_wrapper.v”
- Without modifying the
testbench:
- Run your simulation and then expect
the assertion of ECC error flags as per address and data mask bits provided in the
user_ecc_wrapper.vfile.