7 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

RevisionDateDescription
A09/2024
The following is the list of changes in revision A of the document:
  • The document was migrated to Microchip template.
  • The document number was updated to DS00005549 from AC478.
  • Updated ECC Operation in PCIe section with information related to PCIe SECDED reporting single and double error counts.
  • Removed PCIe block information from Table 1-1 section.
  • Updated Figure 2-1 in the Register Locks section.
4.0—

The following is a summary of changes made in this revision.

3.0—

The following is a summary of changes made in this revision.

Information about SYSCTRL_ACTIVITY port description was updated. See Table 1-2.

Information about PolarFire FPGA export classification was updated. See Table 1-3.

Updated Figure 1-3.

2.0—

Information about System Controller was updated.

1.0—The first publication of this document.