Description
"GENERATEPROGRAMMINGDATA" is the name of a command tool used in the run_tool command. The "run_tool -name {GENERATEPROGRAMMINGDATA}" Tcl command generates the files needed for generating programming bitstream files.
run_tool -name {GENERATEPROGRAMMINGDATA}
Arguments
Parameter | Type | Description |
---|
None | None | None |
Return Type | Description |
---|
Integer | Returns 0 on success and 1 on failure. |
Error Codes
Error Code | Description |
---|
None | None |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command generats programming bitstream file:
run_tool -name {GENERATEPROGRAMMINGDATA}