Description
"EXPORTNETLIST" is a command tool used in the run_tool command. This command exports a
*.v
or *.vhd
netlist file to the active
synthesis implementation folder.
run_tool -name {EXPORTNETLIST}
Arguments
Parameter | Type | Description |
---|
None | None | None |
Return Type | Description |
---|
Integer | Returns 0 on success and 1 on failure. |
Error Codes
Error Code | Description |
---|
None | None |
Supported Families
Supported Families |
PolarFire® |
PolarFire SoC |
RTG4™ |
SmartFusion® 2 |
IGLOO® 2 |
Example
The following command exports netlist file:
run_tool -name {EXPORTNETLIST}