5.12 Handoff Design for Debugging
(Ask a Question)5.12.1 Exporting SmartDebug Data
(Ask a Question)- In the Design Flow window, expand Handoff Design for Production.
- Expand Handoff Design for Debugging, right-click Export SmartDebug Data, and click Export. The Export SmartDebug Data dialog box appears.
- Select the design debug data
(
*.ddc
) file you want to export.
You can use this file to create a stand-alone SmartDebug project (see the following figure for an example).
Field | Description |
---|---|
Name | Name of the design. |
Location | Location of the exported debug file. By default, the
*.ddc file has the *.ddc file
extension and exports to the
<project_location>/designer/<design>/export
folder. |
Existing design debug data files | You can export *.ddc files in the export folder
after running Generate FPGA Array Data for the design in the Libero® Design Flow. You can also export
SmartDebug data directly after running Synthesize on the design.
Other tools, such as Place and Route and Generate FPGA Array Data)
are run implicitly before the Export SmartDebug Data dialog box is
displayed. |
Include design components | A *.ddc file can contain the following
components:
|
Include security components |
This field is supported for PolarFire® only.
If DPK is selected, DPK is passed to (*.ddc) for unlocking the debug features. Similarly, if UPK1 is selected, UPK1 is passed to (*.ddc) for unlocking the debug features. If both DPK and UPK1 are selected, both are passed to (*ddc), but only DPK is used for unlocking the debug features. If DPK is permanently disabled, UPK1 is used for unlocking the device. |
Programming Options set with the Configure Programming Options tool | Read-only values that show the design version and back level
version set in the Configure Programming Options Wizard. From these values, you can use the bitstream file information for programming the device in Standalone SmartDebug. Note: Info and
warning messages appear based on the value set for the back
level version.
|
Include bitstream file to program at trusted facility | SmartFusion 2, IGLOO 2, and RTG4 only. Choices are:
|