3.5.1.1.4 Data Flow (Streaming) Parallelism
(Ask a Question)The second style of coarse-grained parallelism is referred to as data flow parallelism. This form of parallelism arises frequently in streaming applications, and are commonly used for video/audio processing, machine learning, and computational finance. In such applications, there is a stream of input data that is fed into the application at regular intervals. For example, in an audio processing application, a digital audio sample may be given to the circuit every clock cycle. In streaming applications, a succession of computational tasks is executed on the stream of input data, producing a stream of output data. For example, the first task may be to filter the input audio to remove high-frequency components. Subsequently, a second task may receive the filtered audio, and boost the bass low-frequency components. Observe that, in such a scenario, the two tasks may be overlapped with one another. Input samples are continuously received by the first task and given to the second task.
SmartHLS provides a way for a developer to specify data flow parallelism through the use of function pipelining (see 3.5.1.9 Function Pipelining) and/or threads (see 3.5.1.13 Data Flow Parallelism with SmartHLS Threads) with SmartHLS's FIFO library (see 3.5.1.17.1 Streaming Library) used to connect the streaming modules.