4.6.27 Warning: Failed to Contact Web Repositories
(Ask a Question)Symptom: The following warning message appears in the Libero
catalog window:
Warning: Failed to contact Web Repositories
Cause: This message can occur for any of the following reasons:
- You do not have a connection to the Internet.
- You do not have write permission to the disk location you have set your vault to.
- Your vault location runs out of disk space. (For
the Linux environment, The Libero vault location is set by default to your user
directory in
~/.actel/vault
. If your work site imposes quota restrictions on the size of user directories, you user directory may run out of disk space). - A firewall prevents access to the Web
Repositories. Resolution: Perform the following procedure:
- Check that you have an Internet connection.
- Check that you have write permission to the vault location or change your vault location setting to a location to which you have write permission ( ).
- Increase the disk space for the vault location to a minimum of 850 MB.
- Contact your IT department about firewall issues.