4.6.34 Wind/U Error: Failed to connect to the registry on server
(Ask a Question)Symptom: The following error message appears:
Wind/U Error: Failed to connect to the registry on server [server_name]
Cause: There might be a Linux security setting that is preventing Libero from connecting to the Wind/U Registry. Typically, this connection is made using a TCP port.
Resolution: Perform the following procedure:
-
Modify the Linux security settings. For example, on RHEL5, navigate to the desktop menu Security Setting Deny TCP connections to Xserver.
, and uncheck - Restart your computer to apply the changes.