1.66 TrustZone Basic with Secure Boot Demonstration - PIC32CMLS60
This example application performs Add and Multiply math operations in Secure Flash BOOT and APPLICATION regions called through veneers in Non Secure Flash APPLICATION region. The LED0 (Green) is switched on in Boot Secure application and the LED1 (Red) in Secure application.
For this example:
- BOCOR.BOOTOPT = 0x3, which means the HMAC with BOOTKEY Secure Boot Verification Method is applied at start-up
- BOCOR.BOOTKEY filled with 1’s
- Performance Level 2 (PL2) is selected
Description
This example is based on trustZone_basic example and provides a Boot Secure project in addition to the Secure and Non-Secure projects to demonstrate Secure Boot feature capability over TrustZone feature.
The TrustZone basic with Secure Boot demonstration then provides two project groups:
- BS_App: Contains Boot Secure and Dummy projects (containing respectively _Secure and _Non-Secure suffixes in project name). – The Dummy project is not used but is kept for H3 project architecture considerations. – Boot Secure project implements math functions (add and multiply as example) and switch on the on-board LED0 (Green) on the BOOT region.
- App: Contains Secure and Non-Secure projects. – Secure project implements math functions (add and multiply as example) and switch on the on-board LED1 (Red) on the Secure APPLICATION region. – Non-secure project uses the math functions on the Non-Secure APPLICATION region exposed by Boot Secure and Secure projects for math operations through veneers.
Components Used
- LED0 (Green) Configured as Secure pin (in BOOT region)
- LED1 (Red) Configured as Secure pin (in APPLICATION region)
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
| Type | Path |
|---|---|
| Project Group | apps/trustZone/trustZone_basic_SBoot_ls60/BS_App |
| Boot Secure Project | apps/trustZone/trustZone_basic_SBoot_ls60/BS_App/Secure/firmware |
| Dummy Project | apps/trustZone/trustZone_basic_SBoot_ls60/BS_App/NonSecure/firmware |
| Project Group | apps/trustZone/trustZone_basic_SBoot_ls60/App |
| Secure Project | apps/trustZone/trustZone_basic_SBoot_ls60/App/Secure/firmware |
| Non-Secure Project | apps/trustZone/trustZone_basic_SBoot_ls60/App/NonSecure/firmware |
| Project Name | Description |
|---|---|
| pic32cm_ls60_Secure.X pic32cm_ls60_cpro_NonSecure.X | Secure and Non-Secure MPLABX projects from BS_App folder for PIC32CM LS60 Curiosity Pro Evaluation Kit |
| pic32cm_ls60_Secure.X pic32cm_ls60_cpro_NonSecure.X | Secure and Non-Secure MPLABX projects from App folder for PIC32CM LS60 Curiosity Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board |
|---|---|
| pic32cm_ls60_Secure.X pic32cm_ls60_cpro_NonSecure.X | PIC32CM LS60 Curiosity Pro Evaluation Kit |
| pic32cm_ls60_cpro_Secure.X pic32cm_ls60_cpro_NonSecure.X | PIC32CM LS60 Curiosity Pro Evaluation Kit |
Setting Up PIC32CM LS60 Curiosity Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Open the App and BS_App projects group in the MPLAB X IDE
- Set the non-secure project (trustZone_basic_with_secureboot_pic32cm_ls60_cpro_NonSecure) as main project then flash the application
- Build and program the application
- Set the Boot Secure project (trustZone_basic_with_secureboot_BS_pic32cm_ls60_cpro_Secure) as main project. Go to Project Properties > EDBG > Program Options > Uncheck “Erase All Before Program” option.
- Build and program the application
- The two on-board LEDs should switch on with a delay due to the Secure Boot
Verification and the math operations are performed in Non-Secure application
Note: The application can be launched in debug mode to do step-by-step and observe how the jumps from non-secure project to secure project only are performed.