1.56 TrustZone Systick Periodic Timeout - PIC32CMLS60
This example application shows how to use the SysTick to generate periodic interrupts on both Secure and Non-secure modes.
Description
This demonstrates TrustZone feature and uses two projects viz., Secure and Non-Secure Project that work together on the same MCU and offering security isolation between the Trusted and the Non-trusted resources in the device.
- Secure project uses secure SysTick timer to generate periodic interrupt every 50ms to toggle a GPIO pin and an LED0
- Non-secure project uses non-secure SysTick timer to generate periodic interrupt every 100ms to toggle a GPIO pin and an LED1
Components Used
- Systick - Secure and non-secure systicks
- LED0 - Configured as secure mode
- LED1 - Configured as non-secure mode
- SECURE_PIN and NON_SECURE_PIN - Configured as secure and non-secure mode respectively
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
| Type | Path |
|---|---|
| Project Group | apps/trustZone/systick/systick_periodic_timeout_ls60 |
| Secure Project | apps/trustZone/systick/systick_periodic_timeout_ls60/Secure/firmware |
| Non-Secure Project | apps/trustZone/systick/systick_periodic_timeout_ls60/NonSecure/firmware |
| Project Name | Description |
|---|---|
| pic32cm_ls60_cpro_Secure.X pic32cm_ls60_cpro_NonSecure.X | Secure and Non-secure MPLABX project for PIC32CM LS60 Curiosity Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board |
|---|---|
| pic32cm_ls60_cpro_Secure.X pic32cm_ls60_cpro_NonSecure.X | PIC32CM LS60 Curiosity Pro Evaluation Kit |
Setting Up PIC32CM LS60 Curiosity Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
- Connect an oscilloscope/Logic analyzer to monitor the PORT pin PA10 (Pin #5 on EXT1)
- Connect an oscilloscope/Logic analyzer to monitor the PORT pin PA11 (Pin #6 on EXT1)
Running the Application
- Open the project group in the MPLAB X IDE and set the non-secure project as main project
- Build and program the application
- Observe the output for PIC32CM LS60 Curiosity Pro Evaluation Kit as follows:
- LED0(Green) and PA10 (Secure pin) is toggled every ~50ms in secure project.
- LED1(Red) and PA11 (Non-secure pin) is toggled every ~100ms in
non-secure project