DRV_ETHPHY_VendorDataSet Function
C
DRV_ETHPHY_RESULT DRV_ETHPHY_VendorDataSet(DRV_HANDLE handle, uint32_t vendorData);
Returns
DRV_ETHPHY_RES_OK - if the vendor data is stored in the client object DRV_ETHPHY_RES_HANDLE_ERR - handle error
Description
This function returns the current value of the vendor data. Each DRV_ETHPHY client object maintains data that could be used for vendor specific operations. This routine allows retrieving of the vendor specific data.
Remarks
The PHY driver will clear the vendor specific data before any call to a vendor specific routine. Otherwise the PHY driver functions do not touch this value. The DRV_ETHPHY_VendorDataGet can be used for reading data into this field. Currently only a 32 bit value is supported. The function is intended for implementing vendor specific functions, like DRV_EXTPHY_MIIConfigure and DRV_EXTPHY_MDIXConfigure, that need a way of maintaining their own data and state machine.
Preconditions
The DRV_ETHPHY_Initialize routine must have been called.
DRV_ETHPHY_Open must have been called to obtain a valid device handle.
DRV_ETHPHY_Setup must have been called to properly configure the PHY