DRV_ETHPHY_ClientOperationAbort Function

C

DRV_ETHPHY_RESULT DRV_ETHPHY_ClientOperationAbort(DRV_HANDLE handle); 

Returns

  • DRV_ETHPHY_RESULT value describing the current operation result: DRV_ETHPHY_RES_OK for success; operation has been aborted an DRV_ETHPHY_RESULT error code if the operation failed.

Description

Aborts a current client operation initiated by the Ethernet PHY driver.

Remarks

None

Preconditions

  • The DRV_ETHPHY_Initialize routine must have been called.

  • DRV_ETHPHY_Open must have been called to obtain a valid opened device handle.

  • A driver operation was started