DRV_ETHPHY_Close Function

C

void DRV_ETHPHY_Close(DRV_HANDLE handle); 

Returns

None

Description

This function closes an opened instance of the Ethernet PHY driver, invalidating the handle.

Remarks

  • After calling this routine, the handle passed in "handle" must not be used with any of the remaining driver routines. A new handle must be obtained by calling DRV_ETHPHY_Open before the caller may use the driver again.

  • Usually there is no need for the driver client to verify that the Close operation has completed.

Preconditions

The DRV_ETHPHY_Initialize routine must have been called for the specified Ethernet PHY driver instance. DRV_ETHPHY_Open must have been called to obtain a valid opened device handle.