DRV_ETHPHY_ClientOperationResult Function
C
DRV_ETHPHY_RESULT DRV_ETHPHY_ClientOperationResult(DRV_HANDLE handle);
Returns
DRV_ETHPHY_RESULT value describing the current operation result: DRV_ETHPHY_RES_OK for success; operation has been completed successfully DRV_ETHPHY_RES_PENDING operation is in progress an DRV_ETHPHY_RESULT error code if the operation failed.
Description
Returns the result of a client operation initiated by the Ethernet PHY driver.
Remarks
This function will not block for hardware access and will immediately return the current status. This function returns the result of the last driver operation. It will return DRV_ETHPHY_RES_PENDING if an operation is still in progress. Otherwise a DRV_ETHPHY_RESULT describing the operation outcome.
Preconditions
The DRV_ETHPHY_Initialize routine must have been called.
DRV_ETHPHY_Open must have been called to obtain a valid opened device handle.
A driver operation was started and completed