4.11.2 The Vertical Scale
The vertical scale resolution and limits are defined in signal definition. The vertical resolution is the difference between the maximum value and minimum value.
Note: Maximum and minimum values are used to create a resolution of
the plot. This does not mean that values higher than Maximum Plot Values or lower than
Minimum Plot Values will not be plotted.
To adjust the position of the graph on the display, use the mouse cursor to hover over the respective signal scale that is displayed on the left and use the scroll wheel to move the display up and down.