4.6.1.12 Ivt Option
The -mivt=address option selects the interrupt
vector table that will be used at the beginning of program execution for those PIC18
devices that implement interrupt vector tables.
The address argument specified is written to the IVTBASE register during
startup, for example, -mivt=0x200 will select the interrupt vector table
whose base address is at 200h. The table at the address you specify must be populated by
vectors in your source code. This is achieved using the base argument in
the interrupt routine definitions you write (see Interrupt Service Routines). The default operation
is to leave the vector table at address 0x8 and this can be made explicit using the option
-mno-ivt.