Configure the SNMPv3 view table on the SNMPv3 View Configuration
page, as shown in the following figure. The entry index keys are View
Name and OID Subtree.Figure 4-9. SNMPv3 View
Configuration
The SNMPv3 View Configuration page has the following
parameters:
Delete: Check to delete the
entry. It is deleted during the next save.
View Name: A string
identifying the view name belonging to this entry. The allowed string length is 1 to
32 and the allowed content is ASCII characters from 33 to 126.
View Type: Indicates the view
type belonging to this entry. Possible view types are:
Included: An optional flag to indicate that this
view subtree must be included
Excluded: An optional flag to indicate that this
view subtree must be excluded
OID Subtree: The OID defines
the root of the subtree to add to the named view. The allowed OID length is 1 to
128. The allowed string content is digital number or asterisk (*).