28.2.61 __builtin_section_begin, __builtin_section_end
Description
Get run-time information about a section beginning or ending address.
Prototype
uint32_t __builtin_section_begin(“section_name”);
uint32_t __builtin_section_end(“section_name”);
Argument
section_name – name of the section
Return Value
Returns the beginning or ending address of the named section.
Assembler Operator
.startof.
.endof.
Error Messages
An error message will be displayed if the named section cannot be found.