28.2.4 __builtin_addr_low, __builtin_addr_high, __builtin_addr
Description
Determine the offset address of a symbol.
Prototype
uint16_t __builtin_addr_low(&symbol);
uint16_t __builtin_addr_high(&symbol);
uint16_t __builtin_addr(&symbol);
Argument
&symbol – The literal address of the symbol
Return Value
Returns the low, high or full address of a symbol, without any adjustment for physical address paging requirements. Therefore, the values returned represent a literal offset and cannot be used for addressing purposes without manipulation.
Machine Instruction
mov.w
(or a pair of mov.w instructions for
__builtin_addr)
Error Messages
An error message will be displayed if the argument is not a literal address.