28.2.64 __builtin_sftac
Description
Shifts accumulator by shift. The valid shift range is
-16 to 16.
For example:
volatile register int16_t result asm(“A”);
int16_t i;
result = __builtin_sftac(result,i);
Might generate:
sftac A, w0
Prototype
int16_t __builtin_sftac(int16_t Accum, int16_t shift);
Arguments
Accum – Accumulator to shift.
shift – Amount to shift.
Return Value
Returns the shifted result to an accumulator.
Machine Instruction
sftac
Error Messages
An error message will be displayed if:
- the result is not an accumulator register
Accumis not an accumulator register- the shift value is not a literal within range