28.2.62 __builtin_section_size
Description
Get run-time information about a section’s size.
Prototype
uint32_t __builtin_section_size(“section_name”);
Argument
section_name – name of the section
Return Value
Returns the size of the named section.
Assembler Operator
.sizeof.
Error Messages
An error message will be displayed if the named section cannot be found.