29.2.19 __builtin_divud

Description

Computes the quotient num / den. A math error exception occurs if den is zero. Function arguments are unsigned, as is the function result. The command-line option -Wconversions can be used to detect unexpected sign conversions.

Prototype

uint16_t __builtin_divud(const uint32_t num, const uint16_t den);

Arguments

num – numerator

den – denominator

Return Value

Returns the unsigned integer value of the quotient num / den.

Assembler Operator/ Machine Instruction

div.ud