29.2.25 __builtin_edspage

Description

Returns the eds page number of the object whose address is given as a parameter. The argument p must be the address of an object in an Extended Data Space (EDS); otherwise an error message is produced and the compilation fails. See the space attribute in 9.11 Variable Attributes.

Prototype

uint16_t __builtin_edspage(const void *p);

Argument

p – literal address of an object

Return Value

Returns the eds page number of the object whose address is given as a parameter.

Assembler Operator

edspage

Error Messages

The following error message is produced when this function is used incorrectly:

“Argument to __builtin_edspage() is not the address of an object in extended data space.”

The argument must be an explicit object address.

For example, if obj is object in an executable or read-only section, the following syntax is valid:

uint16_t page = __builtin_edspage(&obj);