29.2.1 __builtin_ACCL, __builtin_ACCH, __builtin_ACCU

Description

Access the value in the low, high, or upper portion of an accumulator. An example for dsPIC33E:

volatile register int value asm(“A”);
int16_t value;

int16_t result = __builtin_ACCL(value);

The example result will be the low 16-bits stored in the accumulator which holds value.

These builtins allow access to the parts of an accumulator in a way that is optimizer safe.

Prototype

int16_t __builtin_ACCL(int16_t value);
int16_t __builtin_ACCH(int16_t value);
int16_t __builtin_ACCU(int16_t value);

Argument

value – Integer number to set accumulator value.

Return Value

Returns the low, high or upper portion of the accumulator.

Machine Instruction

mov.w

Error Messages

An error message will be generated if the current target does not support DSP instructions.