29.2.40 __builtin_mac
Description
Computes a x b and sums with accumulator;
also prefetches data ready for a future MAC operation.
xptr may be null to signify no X prefetch to be performed, in
which case the values of xincr and xval
are ignored, but required.
yptr may be null to signify no Y prefetch to be performed, in
which case the values of yincr and yval
are ignored, but required.
xval and yval nominate the address of a C
variable where the prefetched value will be stored.
xincr and yincr may be the literal
values: -6, -4, -2, 0, 2, 4, 6 or an integer value.
If AWB is non null, the other accumulator will be written back
into the referenced variable.
For example:
volatile register int16_t result asm("A");
volatile register int16_t B asm("B");
int16_t *xmemory;
int16_t *ymemory;
int16_t xVal, yVal;
result = __builtin_mac(result, xVal, yVal, &xmemory, &xVal, 2, &ymemory, &yVal, 2, 0, B);
might generate:
mac w4*w5, A, [w8]+=2, w4, [w10]+=2, w5
Prototype
int16_t __builtin_mac(int16_t Accum, int16_t a, int16_t b,
int16_t **xptr, int16_t *xval, int16_t xincr,
int16_t **yptr, int16_t *yval, int16_t yincr,
int16_t *AWB, int16_t AWB_accum);
Arguments
Accum – Accumulator to sum.
a – Integer multiplicand.
b – Integer multiplier.
xptr – Integer pointer to pointer to x prefetch.
xval – Integer pointer to value of x prefetch.
xincr – Integer increment value of x prefetch.
yptr – Integer pointer to pointer to y prefetch.
yval – Integer pointer to value of y prefetch.
yincr – Integer increment value of y prefetch.
AWB – Accumulator write back location.
AWB_accum – Accumulator to write back.
Return Value
Returns the value of accumulator plus the result of a x b.
Machine Instruction
mac
Error Messages
An error message will be displayed if:
- the result is not an accumulator register
Accumis not an accumulator registerxvalis a null value butxptris not nullyvalis a null value butyptris not nullAWB_accumis not an accumulator register andAWBis not null