29.2.7 __builtin_btg
Description
This function will generate a btg machine instruction.
Some examples include:
int16_t i; /* near by default */
int16_t l attribute((far));
struct foo {
int16_t bit1:1;
} barbits;
int16_t bar;
void some_bittoggles() {
register int16_t j asm("w9");
int16_t k;
k = i;
__builtin_btg(&i,1);
__builtin_btg(&j,3);
__builtin_btg(&k,4);
__builtin_btg(&l,11);
return j+k;
}
Note: Taking the address of a variable in a register will produce
warning by the compiler and cause the register to be saved onto the stack (so that its
address may be taken); this form is not recommended. This caution only applies to
variables explicitly placed in registers by the programmer.
Prototype
void __builtin_btg(uint16_t *, uint16_t 0xn);
Arguments
* – A pointer to the data item for which a bit should
be toggled.
0xn – A literal value in the range of 0 to 15.
Return Value
Returns a btg machine instruction.
Machine Instruction
btg
Error Messages
An error message will be displayed if the parameter values are not within range.