29.2.83 __builtin_subab
Description
Subtracts accumulators A and B with the result written back to the specified accumulator.
For example:
volatile register int16_t result asm("A");
volatile register int16_t B asm("B");
result = __builtin_subab(result,B);
will generate:
sub A
Prototype
int16_t __builtin_subab(int16_t Accum_a, int16_t Accum_b);
Arguments
Accum_a – Accumulator from which to subtract.
Accum_b – Accumulator to subtract.
Return Value
Returns the subtraction result to an accumulator.
Machine Instruction
sub
Error Messages
An error message will be displayed if the result is not an accumulator register.