2.1.4.5 Calculation for Heat Sink
(Ask a Question)For example, in a design implemented in an A2F500-FG484 package with 2.5 m/s airflow, the power consumption value using the power calculator is 3W. The user-dependent Ta and Tj are given as follows:
TJ = 100.00 °C
TA = 70.00 °C
From the datasheet:
θJA = 16.4 °C/W
θJC = 7.5 °C/W
The 1.82 W power is less than the required 3.00 W. The design therefore requires a heat sink, or the airflow where the device is mounted should be increased. The design's total junction-to-air thermal resistance requirement can be estimated by Calculation for Heat Sink:
Determining the heat sink's thermal performance proceeds as follows:
where:
θJA = 0.37°C/W
= Thermal resistance of the interface material between the case and the heat sink, usually provided by the thermal interface manufacturer
θSA = Thermal resistance of the heat sink in °C/W
A heat sink with a thermal resistance of 2.5 °C/W or better should be used. Thermal resistance of heat sinks is a function of airflow. The heat sink performance can be significantly improved with increased airflow.
Carefully estimating thermal resistance is important in the long-term reliability of an FPGA. Design engineers should always correlate the power consumption of the device with the maximum allowable power dissipation of the package selected for that device.