6.2.1 Nonvolatile Memory (NVM) Control Register

Note:
  1. A BOR event Reset will indirectly clear WR by forcing the FSM to terminate the operation underway. The WR bit cannot be set if the operation target address held in the NVMADRx register falls within unimplemented address space.
  2. Reset only on POR or BOR, but the actual initial state of P2ACTIV visible to the user will depend upon which panel is determined to be active after Reset exit.
  3. A BMX address error is likely due to a bad NVMSRCADR value. The same error will generate a bus error TRAP via the interrupt controller. This will aid the software in diagnosing the issue.
  4. The WRERR bit will remain set if an attempt is made to execute (WR=1) a reserved PROGOP command. The WR bit will not remain set.
  5. “Word” is defined to be a 128-bit data value plus ECC (140 bits total). However, each word program command may consist of a sequence of fractional word programming operations.
  6. Reserved when in Single Boot mode (DUAL_BOOTPRESENT=0).
Name: NVMCON
Offset: 0x3000

Legend: x = bit is unknown; R = Readable bit; W = Writable bit; HC = Hardware Clearable bit; HS = Hardware Settable bit; C = Clearable bit; S = Settable bit

Bit 3130292827262524 
          
Access  
Reset  
Bit 2322212019181716 
    WRRE WREC[2:0] 
Access R/HS/HCR/HS/HCR/HS/HCR/HS/HC 
Reset 0000 
Bit 15141312111098 
 WRWRENWRERRNVMPIDLSFTSWPP2ACTIV   
Access R/SOR/WR/WR/WR/CR 
Reset 00000x 
Bit 76543210 
 LOCKDRBV  NVMOP[3:0] 
Access R/SR/HS/CR/WR/WR/WR/W 
Reset 000000 

Bit 20 – WRRE Program/Erase Reset Event bit

ValueDescription
1 Warm Reset request during program/erase operation.
0 No event reported.

Write 0 to clear, writing 1 has no effect.

Bits 18:16 – WREC[2:0] Program/Erase Error Code bits

ValueDescription
101 Row Programming operation is not completed due to warm Reset.
100 System bus error during a Row Program operation.
011 Error reported by Flash panel control logic.
010 Security access control violation.
001 Invalid Program/Erase operation (PROGOP)
000

No error.

Unused codes are reserved.

Read as ‘0’ if WRERR=0.

Bit 15 – WR  Write Control bit(1)

ValueDescription
1 Initiates a memory or fuse element Program or Erase operation.
0 Program or Erase operation is complete and inactive.

Bit 14 – WREN Program/Erase Enable bit

ValueDescription
1 Allows program/erase cycles.
0 Inhibits programming/erasing of memory or fuse elements. This bit cannot be updated if either the LOCK bit is set or the WR bit is set.

Bit 13 – WRERR Sequence Error Flag bit

ValueDescription
1
Indicates an improper program or erase termination due to:
  • An attempt to execute a reserved PROGOP command.
  • An error detected by the Smart Write module such as Flash failures.
  • If a BMX address error is detected during a Row Programming operation.

This bit cannot be set by software.

0

Either a POR or BOR has occurred or software cleared the WRERR bit.

Bit 12 – NVMPIDL NVM Power Down in Idle Enable bit

ValueDescription
1

Flash panels enter a Sleep mode (very Low-Power mode) when device enters Idle mode.

0 Keep Flash and fuse panels powered in Standby mode when the device enters Idle mode.

Bit 11 – SFTSWP Soft Swap Status bit

ValueDescription
1

When Dual Boot Mode is present:

Panels have been successfully swapped using the BOOTSWP instruction.

0

Awaiting successful panel swap using the BOOTSWP instruction.

Write 0 to clear; writing 1 has no effect. Read as ‘0’ in single boot mode.

Bit 10 – P2ACTIV  Dual Boot Active Region Status bit(2)

ValueDescription
1

When Dual Boot Mode is present:

Panel 2 is mapped into active region.

0

Panel 1 is mapped into active region.

Read as '0' in single boot mode.

Bit 7 – LOCK Lock bit

ValueDescription
1 Program/erase functions are disabled until after the next Reset.
0

Program/erase functions are not disabled.

Write 1 to set, writing 0 has no effect.

Bit 6 – DRBV Data Read Buffer Valid bit

ValueDescription
1 Data read buffer holds valid data.
0

Data read buffer invalid

Write 0 to clear, writing 1 has no effect.

Bits 3:0 – NVMOP[3:0]  NVM Operation Select bits(3,4,5,6)

ValueDescription
0111-0101 Reserved
0100 Next WR command performs an Inactive Partition Erase operation.
0011 The next WR command will perform a memory Page Erase operation.
0010 The next WR command will perform a Row Program 1 operation.
0001 The next WR command will perform a Word Program 1, 3 operation (data source: NVMDATAx).
0000 Reserved