13.1.3 View Menu
This section lists the menu items in the View menu.
For keyboard shortcuts of some of these menu items, see .
| Command | Action |
|---|---|
| Editors | Selects an
available editor to view your files.
|
| Split | Splits the current editor window and its contents into two windows, either Vertically or Horizontally oriented. Select Clear to remove the selection. |
| If the insertion point is in a foldable section of text, collapses those lines into one line. | |
| If the currently selected line in the Source Editor represents several folded lines, expands the fold to show all of the lines. | |
| Collapses all foldable sections of text in the Source Editor. | |
| Expands all foldable sections of text in the Source Editor. | |
| Collapses all folds in a nested group of folds. | |
| Expand all folds in a nested group of folds. | |
| IDE Log | Opens the log file in a tab of the Output window. |
| , etc. | Shows the associated toolbar. |
| Uses small icons on the toolbars. | |
| Resets to the default toolbar setup. | |
| Customizes the items on an existing toolbar and allows creation of a new one. | |
| Show Editor Toolbar | Shows the editor toolbar on the File tab. |
| Show Line Numbers | Shows line numbers in left margin. |
| Show Non-printable Characters | Shows characters even if they are not printable (non-ASCII). |
| Show Breadcrumbs | Shows breadcrumbs, or the path to the file from the project file, on the bottom of the editor window. |
| Show Indent Guide Lines | Shows faint lines to represent indents. |
| Show Diff Sidebar | Shows the DIFF sidebar. |
| Show Versioning Labels | Shows version labels. |
| Synchronize Editor with Views | Synchronizes the editor with open views. |
| Show Only Editor | Shows editor window in full IDE window. |
| Full Screen | Expands window to full length and breadth of screen. |