13.1.4 Navigate Menu
This section lists the menu items in the Navigate menu.
For keyboard shortcuts of some of these menu items, see .
| Command | Action |
|---|---|
| Go to File | Finds and opens a specific file. |
| Go to Type | Finds and opens a specific class or interface. |
| Go to Symbol | Finds the symbol name as specified. |
| Go to Previous Window | Gives focus to the previously selected window. |
| Go to Source | Displays the source file containing the definition of the selected class. |
| Go to Declaration\Definition | Jumps to the declaration or definition of the item under the cursor. |
| Go to Super Implementation | Jumps to the super implementation of the item under the cursor. |
| Last Edit Location | Scrolls the editor to the last place where editing occurred. |
| Back | Navigates back. |
| Forward | Navigates forward. |
| Go to Line | Jumps to the specified line. |
| Toggle Bookmark | Sets a bookmark on a line of code. |
| Bookmark History Popup Next | Goes to the next bookmark in the Bookmark window (). |
| Bookmark History Popup Previous | Goes to the previous bookmark in the Bookmark window (). |
| Next Error | Scrolls the Source Editor to the line that contains the next build error. |
| Previous Error | Scrolls the Source Editor to the line that contains the previous build error. |
| Select in Projects | Opens the Projects window and selects current document within. |
| Select in Files | Opens the Files window and selects current document within. |
| Select in Classes | Opens the Classes window and selects current document within. |
| Select in Favorites | Opens the Favorites window and selects current document within. |