13.1.8 Debug Menu
Below are the menu items in the Debug menu.
For keyboard shortcuts of some of these menu items, see .
| Command | Action |
|---|---|
| Debug1 | Debugs the main or selected project. |
| Discrete Debugger Operation | Perform the
following debug operations one step at a time (discretely.) This is
useful for changing the Memory window setting during debug and using
starter kits.
If the target is running, you can use: |
| Finish Debugger Session | Ends the debugging session. |
| Pause | Pauses debugging – use Continue to resume. |
| Continue | Resumes debugging after Pause until the next breakpoint or the end of the program is reached. |
| Step Over | Executes one source line of a program. If the line is a function call, executes the entire function and then stops. |
| Step Into | Executes one source line of a program. If the line is a function call, it executes the program up to the function’s first statement and then stops. |
| Step Out | Executes one source line of a program. Finishes execution of the current function and stops on the source line immediately following the call to that function. |
| Step Instruction | Executes one machine instruction If the instruction is a function call, it executes the function and returns control to the caller. |
| Run to Cursor | Runs the current project to the cursor’s location in the file and stop program execution. |
| Reset | Resets the device. |
| Set PC at cursor | Sets the program counter (PC) value to the line address of the cursor. |
| Focus Cursor at PC | Moves the cursor to the current PC address and centers this address in the window. |
| Makes the method being called the current call . Only available when a call is selected in the Call Stack window. | |
| Makes the calling method the current call. Only available when a call is selected in the Call Stack window. | |
| Pops the call on top of the stack. | |
| Pops the current stack from the top of the stack. | |
| Pops the last call from the debug tool from the top of stack. | |
| Toggle Line Breakpoint | Adds a line breakpoint or removes the breakpoint at the cursor location in the program. |
| New Breakpoint | Sets a new breakpoint at the specified line, exception, or method. |
| New Watch | Adds the specified symbol to watch. |
| New Run Time Watch | Adds the specified symbol to watch that will change value as the program runs/executes. |
| Disconnect from Debug Tool | Disconnects communications between MPLAB X IDE and the debug tool. To reconnect, either Run or Debug. |
| Run Debugger/Programmer Self Test | Performs a debug tool self-test. For tools that support a self test, follow the tool documentation to set up the hardware and then run this test to confirm proper operation. |
| Hardware Tool Emergency Boot Firmware Recovery | Run utility to restore hardware tool boot firmware to its factory state. See MPLAB ICE x, MPLAB ICD x or MPLAB PICkit x documentation for details, where x = 4 or 5. |
| |