13.1.6 Refactor Menu
This section lists the menu items in the Refactor menu. The items you see are dependent on the type of object (variable, function, etc.) you are refactoring. For more information, see C Code Refactoring.
For keyboard shortcuts of some of these menu items, see .
| Command | Action |
|---|---|
| Rename | Enables you to change the name of a variable or function to something more meaningful. In addition, it updates all source code in your project to reference the element by its new name. |
| Move | Moves a class to another package or into another class In addition, all source code in your project is updated to reference the class in its new location. |
| Copy | Copies a class to the same or a different package. |
| Safely Delete | Checks for references to a code element and then automatically deletes that element if no other code references it. |
| Change Function Parameter | Changes the amount and name of parameters for the selected function. |
| Introduce Variable / Constant / Field / Method | Select the code you want to be replaced by the variable, constant, field or method. Then select Introduce Your Choice and give it a name in the dialog that opens. |