13.1.5 Source Menu
This section lists the menu items in the Source menu.
For keyboard shortcuts of some of these menu items, see .
| Command | Action |
|---|---|
| Format | Formats the selected code, or the entire file if nothing is selected. |
| Remove Trailing Spaces | Removes spaces at the end of the line. |
| Shift Left | Moves the selected line, or lines one tab to the left. |
| Shift Right | Moves the selected line, or lines one tab to the right. |
| Move Up | Moves the selected line, or lines one line up. |
| Move Down | Moves the selected line, or lines one line down. |
| Move Code Element Up | Moves the selected code element up one line. |
| Move Code Element Down | Moves the selected code element down one line. |
| Duplicate Up | Copies the selected line or lines one line up. |
| Duplicate Down | Copies the selected line or lines one line down. |
| Toggle Comment | Toggles the commenting out of the current line or selected lines. |
| Complete Code | Shows the code completion box. |
| Insert Code | Pops up a context aware menu that you can use to generate common structures such as constructors, getters, and setters. |
| Fix Code | Displays editor hints. The IDE informs you when a hint is available when the light bulb is displayed. |
| Show Method Parameters | Selects the next parameter. You must have a parameter selected (highlighted) for this shortcut to work. |
| Show Documentation | Shows documentation for item under the cursor. |
| Insert Next Matching Word | Generates the next word used elsewhere in your code, as you type its beginning characters. |
| Insert Previous Matching Word | Generates the previous word used elsewhere in your code, as you type its beginning characters. |
| Inspect | Runs the specified inspection on the selected file, package, or project. |
| Scan for External Changes | Scans file for changes made outside of MPLAB X IDE. |