13.1.11 Window Menu
This section lists the menu items in the Window menu.
For keyboard shortcuts of some of these menu items, see .
| Command | Action |
|---|---|
| MPLAB® Code Configurator v5 | Opens MCC v5.
Same action as ![]() |
| Kit Window | Opens the Kit Window. Several kits when connected will be autodetected and the window will open. |
| Projects | Opens the Projects window. |
| MPLAB Discover | Opens MPLAB Discover tab. Same
action as . |
| Files | Opens the Files window. |
| Classes | Opens the Classes window. |
| Favorites | Opens the Favorites window. |
| Services | Opens the
Services window. See NetBeans help for more on this window. |
| Dashboard | Opens the Dashboard window. |
| Navigator | Opens the
Navigator window. See NetBeans help for more on this window. |
| Acton Items | Opens the Action Items window. |
| Tasks | Opens the
Task List window. See NetBeans help for more on this window. |
| Output | Opens or moves to front the Output window. |
| Editor | Opens an empty Editor window. |
| Debugging | Opens debugging windows. |
| Web | Opens web-related windows. |
| IDE Tools | Opens an IDE tools window. |
| Target Memory Views > Memory Type | Opens specified Memory window. Memories shown depend on the project device. See either: |
| Simulator | Opens Simulator windows. |
| Programming Center | Opens the Programming Center
tab. Same action as “Order Free Programmed Samples” on drop-down list. |
| Event Recorder | Opens the Event Recorder List View tab. |
| Configure Window | Configures window(s) according to a listed option. |
| Reset Window | Resets windows to their default settings. |
| Close Window | Closes the current tab in the current window. If the window has no tabs, the whole window is closed. |
| Close All Documents | Closes all open documents in the Source Editor. |
| Close Other Documents | Closes all open documents except the active one. |
| Document Groups | Create named document group(s). |
| Documents | Opens the Documents dialog box, in which you can save and close groups of open documents. |